Hello,
According to datasheet, ADC 10/12-Bit linearity/timing parameters are not described at Vcc 2.0V~.
(Question)
(1) Do you have ADC 10/12-Bit linearity/timing parameters at Vcc 2.0V~ ?
(2) From what power voltage can it support with ADC 10/12-Bit mode?
(3) According to Table 5-20 in datasheet, the following note is described.
“(1) This specifies the ADC functional range with 8-bit resolution at 8-bit ENOB. Table 5-22 specifies 10- and 12-bit linearity parameters for
better ENOB requirements.”
It means it doesn’t meet as ADC 10/12-Bit mode specification at Vcc 2.0V~.
My understanding is correct?
Regards,
Tao_2199