Part Number: MSP430F6736
Other Parts Discussed in Thread: UNIFLASH
Hi experts,
This is the result of checking the original thread.
Is there any possible cause for the difference in behavior between F6736 and F6733 despite writing the same .out file?
We thought that the .out file that was working on F6733 would work on F6736 as well. However, when I checked the behavior after writing on the customer side, there seems to be a difference. Currently, We are trying to create an executable file by creating a new project in the proper way, setting the device information as F6736, and keeping the linker and other settings the same. The difference from the expected behavior is that it is not accepting the startup trigger by UART reception. (UART interrupt is not accepted)
As far as the memory map is concerned, there are differences only in Flash and RAM. We have confirmed that there is no difference in register configuration and errata. The exact information and detailed diffs are currently under confirmation, but I am concerned that I may have missed some fundamental factor. I'm sorry for the lack of information, but I would appreciate it if you could tell me what you think might be the cause.
Best regards,
O.H