This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F437: MSP430 Reading ROM hex over SPI

Part Number: MSP430F437

Hello, 

I got this question regarding the MSP430F437, 100 pin MCU.

"Is it possible to read all data ROM hex out using SPI pins only ?

Pins:

  • TDO/TDI 90
  • TMS 92
  • TCK 93
  • And Power 3.3V and GND
  • do I need to connect also 
    • RST/NMI 94 ?

 

Can data from this ROM be locked? (so no possibility to read it if it was locked ?)"

Best,

Alex

**Attention** This is a public forum