Part Number: MSP430F67671A
Hello
I refer to the following files.
SLAU208Q (MSP430x5xx and MSP430x6xx Family User's Guide)
SLAS983A (MSP430F677x1A Data sheet)
SLAS655G (MSP430F543xA Data sheet)
1. ADC10_A
Figure 27-3 (SLAU208Q)

Table 5-48 (SLAS983A)

It seems that the conversion time is 12clk of ADC10CLK.
On the other hand,
Figure 27-6 (SLAU208Q)

①:Convert : 10 x ADC10CLK
②:Result Stored Into ADC10MEM0, ADC10IFG0 is Set : 1 x ADC10CLK
Q1.
Is not ① 12 x ADC10CLK ?
2. ADC12_A
Figure 28-4 (SLAU208Q)

8.37 12-Bit ADC, Timing Parameters (SLAS655G)

It seems that the conversion time is 13clk of ADC12CLK.
On the other hand,
Figure 28-7 (SLAU208Q)

①:Convert : 12 x ADC12CLK
②:Result Stored Into ADC12MEMx, ADC12IFGx is Set : 1 x ADC12CLK
Q2.
Is not ① 13 x ADC12CLK ?
Best Regards,