Part Number: MSP430F5247
Other Parts Discussed in Thread: MSP430F5257
Hi team,
I would like to understand what changes need to be made to change from MSP430F5247 to MSP430F5257.
Do customer need both hardware and software changes?
Thanks,
Connie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F5247
Other Parts Discussed in Thread: MSP430F5257
Hi team,
I would like to understand what changes need to be made to change from MSP430F5247 to MSP430F5257.
Do customer need both hardware and software changes?
Thanks,
Connie
Hi Connie,
Here is a chart comparing the two devices at a high-level--both the devices are in the same device family (from https://www.ti.com/microcontrollers-mcus-processors/microcontrollers/msp430-micrcontrollers/products.html):
MSP430F5257 |
MSP430F5247 |
||
|---|---|---|---|
| Features | Real-time clock | Real-time clock | |
| ADC | 10-bit SAR | 10-bit SAR | |
| Non-volatile memory (kB) | 128 | 64 | |
| USB | No | No | |
| Special I/O | 1.8V I/O | ||
| GPIO pins (#) | 53 | 53 | |
| Frequency (MHz) | 25 | 25 | |
| RAM (KB) | 16 | 8 | |
| Number of ADC channels | 10 | 10 | |
| UART | 4 | 2 | |
| Number of I2Cs | 4 | 2 | |
| SPI | 8 | 4 | |
| Comparator channels (#) | 8 | 8 | |
| Approx. price (USD) |
$1.990 | 1ku
|
$1.710 | 1ku
|
Are you trying to implement a specific feature across both devices/could you expand more on what you are using the boards for? Changes might need to be made specific to the implementation.
Hi Amruta,
I would like to know if it is a pin to pin replacement without needing hardware changes. The MSP430F5247/9 are both out of stock, so I am trying to find an alternative with least amount of changes needed. Just based on the high level overview, I can't tell what kind of changes would be required.
Could you advise if hardware/software changes are needed to change from F5247 to F5257?
Thanks,
Connie
Hi Connie,
Assuming you are comparing the 64-pin RGC packages of both boards, you can see from the screenshots from the datasheet below that they are similar; however, there are a few differences to note:
Pin Diagram for F5247:

Pin Diagram for F5257:

Hi Amruta,
This is great information! Thanks for digging into this a little further. I may follow up with more questions on port mapping if customer is interested in switching over.
**Attention** This is a public forum