Part Number: MSP430FR5969
Hi,
I have writtern a program for MSP430fr5969 and it works when compiled and debuged in CCS 10 and the program works fine, Now i m working in LDRA cover tool with CCS linker , there it creates an error i have pasted down the error block. I am not able to find why it creates an error
'Building target: "perdaa_7.out"'
'Invoking: MSP430 Linker'
"C:/ti/ccs1020/ccs/tools/compiler/ti-cgt-msp430_20.2.2.LTS/bin/cl430" -vmspx --data_model=restricted --use_hw_mpy=F5 --advice:power=all --advice:hw_config=all --define=__MSP430FR5969__ --define=_MPU_ENABLE -g --printf_support=minimal --diag_warning=225 --diag_wrap=off --display_error_number --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 -z -m"perdaa_7.map" --heap_size=160 --stack_size=160 --cinit_hold_wdt=on -i"C:/ti/ccs1020/ccs/ccs_base/msp430/include" -i"C:/ti/ccs1020/ccs/ccs_base/msp430/lib/5xx_6xx_FRxx" -i"C:/ti/ccs1020/ccs/ccs_base/msp430/lib/FR59xx" -i"C:/ti/ccs1020/ccs/tools/compiler/ti-cgt-msp430_20.2.2.LTS/lib" -i"C:/ti/ccs1020/ccs/tools/compiler/ti-cgt-msp430_20.2.2.LTS/include" --priority --reread_libs --define=_MPU_ENABLE --diag_wrap=off --display_error_number --warn_sections --xml_link_info="perdaa_7_linkInfo.xml" --use_hw_mpy=F5 --rom_model -o "perdaa_7.out" "./built_in_test.obj" "./clock.obj" "./command.obj" "./conversion.obj" "./dose_rate_calculation.obj" "./perdaa_7.obj" "./pwm.obj" "./rtc.obj" "./spi_nand.obj" "./spi_nand1.obj" "./spi_nand2.obj" "./timer_counter.obj" "./uart.obj" "./uart_interrupt.obj" "../lnk_msp430fr5969.cmd" -llibmpu_init.a -llibmath.a -llibc.a
undefined first referenced
symbol in file
--------- ----------------
QQQfcn_ptr_num ./uart_interrupt.obj
ldra_buffer ./uart_interrupt.obj
ldra_port_open ./uart_interrupt.obj
ldra_port_write ./uart_interrupt.obj
ldra_sprintf1 ./uart_interrupt.obj
qqpopulate_array_fcn_ptrQQ ./uart_interrupt.obj
zzopen ./uart_interrupt.obj
error #10234-D: unresolved symbols remain
remark #10372-D: (ULP 4.1) Detected uninitialized Port A in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
remark #10372-D: (ULP 4.1) Detected uninitialized Port B in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
error #10010: errors encountered during linking; "perdaa_7.out" not built
>> Compilation failure
makefile:156: recipe for target 'perdaa_7.out' failed
gmake[1]: *** [perdaa_7.out] Error 1
makefile:152: recipe for target 'all' failed
gmake: *** [all] Error 2
Error: Failed to build the program