Part Number: EVM430-FR6047
Other Parts Discussed in Thread: MSP430FR6047
Hi Team,
We would like to ask your help regarding the customer's inquiry below.
We are experimenting with different methods for flow metering. We have run the evaluation board for the MSP430FR6047 (EVM430-FR6047) using the PC evaluation software. The flow vessel body is non-conventional, it has a double elbow at both the inlet and outlet. This causes some amount of flow turbulence by the time the flow gets to the transducers. The transducers are 2MHz and the pipe size is ¾”. The evaluation board works well at low flows, but at about 14 GPM and above, the MSP430FR6047 does not track flow. The ADC continuous capture display shows a large amount of amplitude variation. Up and down stream amplitudes are somewhat different. Are there any type of parameter configurations to help with the high flow condition?
Regards,
Danilo