Other Parts Discussed in Thread: MSP-TS430PN80A
When driving the XT2IN with a crystal oscillator, what are the duty cycle specifications and the rise/fall times required? Our existing oscillator is 20MHz with a 45% to 55% duty cycle and a 5nsec rise/fall times (when driving a 15pF). A replacement oscillator is the same except the rise/fall times are 10nsec (when driving15pF). Will this alternate crystal oscillator work with the MSP4305329? Is there a minimum high time for the clock? Is there a minimum low time for the clock?