This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2955: IO port simulates UART serial communication, sending and receiving function routines?

Part Number: MSP430G2955
Other Parts Discussed in Thread: ENERGIA

  • Hello, please ask a question:

  • Using chip MSP430G2955, using IO port to simulate UART serial communication,P3.6=Tx,P3.7=Rx. 

    Cannot use timer A (because the hardware UART serial port is already in use),The system clock adopts a built-in clock of 1MHz. The BAUd rate of the I/O port to simulate the UART serial port is 115200.

  •   Hope to provide reference routines, thank you very much!  

  • I am looking forward to your reply. Thank you!  

**Attention** This is a public forum