Other Parts Discussed in Thread: MSP-EXP430FR2355
I read few documents about BSL, I try enter BSL via below code or control RST & TEST pin, I think it works because the firmware stop running. But I fail to communicate with BSL via UART.
__disable_interrupt(); // disable interrupts
((void (*)())0x1000)(); // jump to BSL
I have two questions:
1.Does BSL use UART0 (P1.6,P1.7) or UART1(P4.2,P4.3)?
2.Are there any tool which program MSP-EXP430FR2355 Launch Pad with eZ-FET debug probe via BSL instead of Spy-Bi-Wire so I can monitor the signals during the process?
Thanks a lot!