This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430I2040: EMDC showing blank values under Results

Part Number: MSP430I2040
Other Parts Discussed in Thread: MSP430I2041, MSP430F5529

Hi,

When I download the code generated by EMDC for MSP430I2041 and flash it into the MSP430I2040, I open the EMDC (EVM430-i2040S-SH-1V-1C-50Hz project and click on the "connected" icon, it says HID connected in the bottom. However when I click on the "Results" tab, all voltage, current, energy and all values are blank. It used to work earlier.

The connections are as shown for PC to msp430F5529(HID bridge) to MSP- Isolation board to MSP430I2040S EVM. The code flashed is the code generated for the EVM430-i2040S-1V-1C-50Hz without any changes.

Can you please tell me what the issue is?

thanks and regards,

Rajkumar

**Attention** This is a public forum