Can I use the MSP439FR5994 launchpad to control the power of the Nordic nFR52850 DK?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I use the MSP439FR5994 launchpad to control the power of the Nordic nFR52850 DK?
Hello,
For future posts, please use a more descriptive title.
control the power of the Nordic nFR52850 DK
I couldn't find this device online. If it has an enable pin and the voltage logic levels are the same as the MSP430, then the LaunchPad could be used to enable/disable the Nordic device. Or you could control a load switch that turns on/off the power to the other device.
Have you considered using one of our SimpleLink MCUs?
The simple answer is yes, but the devil is in the details.
Does your controlled chip have an enable?
Does it draw only a few mA?
Can it be powered by the minimum voltage at the current draw that the MSP puts out?
Can you use an external transistor?
Hello,
I've merged your new thread with your existing thread. In the future, please make one post per topic. Thanks.
Sounds like you don't need another MCU at all:
"The nRF52840 is built around the 32-bit ARM® Cortex-M4 CPU with floating point unit running at 64 MHz. "
You should look at some of the TI "CC" chips that will let you use CCS to program them.
Okay, can you recommend something to me? I need BLE communication units as peripherals.
You can find our BLE products here: https://www.ti.com/wireless-connectivity/bluetooth/overview.html
The whole point is that you don't *need* the msp430fr5994, for example, the CC1352 has a 48MHz ARM built in:

**Attention** This is a public forum