This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2355: SFRIFG1 register help?

Part Number: MSP430FR2355

I am running into an issue trying to access the SFRIFG1 register using a HAL approach.  The header file looks like the following:

#ifndef DRIVERS_INC_SFR_H_
#define DRIVERS_INC_SFR_H_

#include <msp430.h>
#include <stdint.h>

typedef struct
{
    volatile uint16_t SFRIE;       /*SFR interrupt enable register                   Offset 0x00 */
    volatile uint16_t SFRIFG;      /*SFR interrupt flag register                     Offset 0x02 */
}SFR_RegDef_t;

#define SFR   (SFR_RegDef_t*)SFR_BASE

typedef struct
{
    SFR_RegDef_t *pSFR; /*holds base address of special function register */
}SFR_Handle_t;


#endif /* DRIVERS_INC_SFR_H_ */

I use this technique on other drivers as well....They all seem to work fine.  For instance when I look at the pointer all working ones point at the correct base address of the register set (ie TB1 points to 0x3C0) as expected.  Here however when I try to access the SFR my debugger points to 0x6904???  This should be 0x0100.  Any thoughts on why this would do this?

My code that is NOT working:

    do
    {
        pECSHandle->pECSx->CSCTL[7] &= ~(XT1OFFG | DCOFFG);
        (clock_SFR.pSFR->SFRIFG) &= ~OFIFG;
    } while ((clock_SFR.pSFR->SFRIFG) & OFIFG);

If I replace (clock_SFR.pSFR->SFRIFG) with SFRIFG1 as in the example Resource Explorer code all is fine.

Thanks

**Attention** This is a public forum