Part Number: MSP430FR2675
I am developing a firmware application based on the demo code for the BOOSTXL-CAPKEYPAD. I have implemented a PWM driver using timer output TA0.1. I added conditional compiles to optionally disable the cap-sense keypad code because it tends to generate spurious interrupts that make debugging of other subsystems difficult. I noticed that the PWM output is very stable when I have the keypad disabled. However, when the keypad is enabled, the PWM output becomes erratic. A cursory review of the keypad driver code indicates that some timer is being used. However, since it's calling into a compiled library, I'm unable to investigate further. How do I figure out which timer the cap-sense keypad driver is using and modify it to use another timer module?