This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2676: Can I have materials related to electrostatic destruction test such as EIAJ, MIL ?

Guru 10570 points
Part Number: MSP430FR2676


Our customer would like to know the result of Electrostatic destruction test.

For example: 

Conditions EIAJ method: C = 200pF, R = 0Ω, 200V or more

MIL method: C = 100pF, R = 1.5kΩ, 1.5kV

(Hope: Presentation of the destruction limit value of each terminal)

Best regards,

RY

**Attention** This is a public forum