This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2355: Problems with I2c BSL and msp430 bsl tool

Part Number: MSP430FR2355


Hello,

I am trying to get the i2c BSL on the MSP430FR2355 to work.  My plan is to update it's firmware via i2c from a raspberry pi.

i installed the msp430 i2cbsl tool on the pi and connected it's i2c bus to pin P1.2 and P1.3 on the MSP. In the MSP Firmware I am invoking the

BSL via software as stated in the datasheet.

This is my code for the BSL invocation. I also made sure that the MSP runs at 8MHz. 

            WDTCTL = WDTPW | WDTHOLD;

            TB3CCR0 = 0x00;         // clear Timer B
            TB3CCTL1 = 0x00;
            TB3CTL = 0x00;

            // Disable all interrupts
            __disable_interrupt();

            FRCTL0 = FRCTLPW | NWAITS_1;
            __bis_SR_register(SCG0);                           // disable FLL
            CSCTL1 = DCORSEL_3;                                // DCO Range = 8MHz
            CSCTL2 = FLLD_0 + 243;                             // DCOCLKDIV = 8MHz
            __delay_cycles(3);
            __bic_SR_register(SCG0);                           // enable FLL

            // Delay after setting clock to invoke BSL
            __delay_cycles(3);

            // Invoke BSL
            ((void (*)() )0x1000)();

After the invocation the BSL is visible on the i2c bus.

But when trying to flash a new firmware it always results in following error:

Any help would be appreciated.

Best regards

Max

**Attention** This is a public forum