Part Number: MSP430G2553
Hello,
I have a little project in interest. In that I would like to sample AIN5 and the chip temperature sequentially 16 times both for filtering. Is it possible? I mean sampling not consequtive channels; or it must be done in two step: sampling 16 times AIN5 and 16 times temperature.
Another question, the compiler gives error on ADC10AE1. Is it; because, they are not pins rather internal connections made with INCH_10 for example? So, ADC10AE registers can not be used sequencing channels?
Regards,
LAszlo