Part Number: MSP430G2553
Hello,
I would like to ask help to convert temperature calibration data to _q5 (11 bit integer part).
I have a long term project needs fast and simple calculation of temperature data. It would be advantageous to have calculate it with the calibration formula. 11 bit integer part fits well to my application where other sensors does not measure higher temperature than 600°C and lower than -40°C; during the calculations 0.03°C precision is far enough.
I highly apriciate your help in advance!
Regards,
Laszlo