Part Number: MSP430FR5989
Hi everyone,
I think I have detected another bug related to the code generated by FlowESI GUI. I think the sampling rate is wrong generated, I have selected a sampling rate frequency of 50 Hz:

But the code generated in the file ../ESIConfig/esiCalibration.c is that:
...
gAFE2Settings = ESI_AFE2_INITPARAMS_DEFAULT;
ESI_AFE2_init(&gAFE2Settings);
gTSMSettings.startTriggerAclkDivider = ESI_TSM_START_TRIGGER_DIV_66;
ESI_TSM_init(&gTSMSettings);
ESI_disableInterrupt(ESI_INTERRUPT_ESISTOP);
}
// DAC Level tester, using Sucessive approx approach
static void AFE2_FindDAC_Fast_Successive(fastParams *fsParam)
{
uint16_t i;
uint16_t dACBit = 0;
...
Therefore, the sampling rate frequency is 32768/66 = 496 Hz.
Mainly, this error affect to the power consumption 9uA vs 3uA.
Would you mind checking that I am right and this is a bug from the FlowESI GUI?
Best regards.