Part Number: MSP430F5438
Dear team,
The customer want to migrating from MSP430F5438A to MSP430F5438 because of (MSP430F5438A) out of stock.
They read the https://www.ti.com/lit/an/slaa419c/slaa419c.pdf and they have several questions.
1 The PMMCOREVx value of MSP430F5438 is only 0 or 2, and cannot be the value of 0,1,2,3
2 How to modify the value of PMMCOREVx in the boot code, and which file to modify?
3 In customer's application, the ADC reference voltage uses the external pin input power supply without using the internal reference voltage, which should have no effect on the AD sampling program. Which peripherals might these reference voltages be used for? Does it has an impact?
4 What is the difference of UCS?

Please help to check these questions.
PS: E2EChina link https://e2echina.ti.com/support/microcontrollers/msp430/f/msp-low-power-microcontroller-forum/208795/msp430f5438
BR,
Susan