Part Number: MSP430FR5969
Hello,
I am new to this forum and a beginner in the msp430 architecture. I want to send data (internal temperature sensor data which is to be transmitted only once at start up) to remote zigbee using msp430 by UART protocol. I was successful in doing that using the launchpad by connecting the zigbee to the 2.0 and 2.1 UART pins for communication. But when I tried to do the same with external power supply (3.3V terminal to VCC and -ve terminal to GND) it doesn't work. It only seemed to work when I was powering up the microcontroller using USB from a PC. Am i doing something wrong or can it be that I am required to use pin 2.5 and 2.6 (eUCSIA1) when giving external power supply. I am attaching the code below:
#include <msp430.h>
#include <stdlib.h>
#include <stdio.h>
#include <string.h>
#include <math.h>
char temp_int_char[5];
char temp_rm_char[5];
char mv_char[5];
char charmemval[] = "ADC12MEM0 Value: ";
char temperature[] = "The Temperature in degree is: ";
char newline[] = " \r\n";
char dot[] = ".";
#define CALADC12_12V_30C *((unsigned int *)0x1A1A) // Temperature Sensor Calibration-30 C
//See device datasheet for TLV table memory mapping
#define CALADC12_12V_85C *((unsigned int *)0x1A1C) // Temperature Sensor Calibration-85 C
unsigned int temp;
volatile float temperatureDegC;
volatile float temperatureDegF;
void ser_output(char *str);
int main(void)
{
volatile float voltage;
int i;
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
CSCTL0_H = CSKEY_H;
CSCTL2 |= SELA__VLOCLK; //Select ACLK to use VLO which runs at about 10KhZ
CSCTL0_H = 0;
P1DIR |= BIT0; //set pin 1.0 as output
P1OUT &= ~BIT0; // set pin 1.0 as low
// P1DIR |= BIT3; //set pin 1.3 as output
// P1OUT |= BIT3; //set pin 1.3 as high
// P1DIR |= BIT2; //set pin 1.2 as output
// P1OUT |= BIT2; //set pin 1.2 as high
// P1DIR |= BIT4; //set pin 1.4 as output
// P1OUT &= ~BIT4; //set pin 1.4 as low
// P4DIR |= BIT6; //set pin 4.6 as output
// P4OUT |= BIT6; //set pin 4.6 as high
initialize_UART();
// Initialize the shared reference module
// By default, REFMSTR=1 => REFCTL is used to configure the internal reference
while(REFCTL0 & REFGENBUSY); // If ref generator busy, WAIT
REFCTL0 |= REFVSEL_0 + REFON; // Enable internal 1.2V reference
/* Initialize ADC12_A */
ADC12CTL0 &= ~ADC12ENC; // Disable ADC12
ADC12CTL0 = ADC12SHT0_8 + ADC12ON; // Set sample time
ADC12CTL1 = ADC12SHP; // Enable sample timer
ADC12CTL3 = ADC12TCMAP; // Enable internal temperature sensor
ADC12MCTL0 = ADC12VRSEL_1 + ADC12INCH_30; // ADC input ch A30 => temp sense
ADC12IER0 = ADC12IE0; // ADC_IFG upon conv result-ADCMEMO
while(!(REFCTL0 & REFGENRDY)); // Wait for reference generator
// to settle
ADC12CTL0 |= ADC12ENC;
ADC12CTL0 |= ADC12SC; // Sampling and conversion start
__bis_SR_register(LPM0_bits | GIE); // LPM0 with interrupts enabled
// __no_operation();
//while(ADC12CTL1 & ADC12BUSY);
int memval = ADC12MEM0;
// Temperature in Celsius. See the Device Descriptor Table section in the
// System Resets, Interrupts, and Operating Modes, System Control Module
// chapter in the device user's guide for background information on the
// used formula.
temperatureDegC = (float)(((long)temp - CALADC12_12V_30C) * (85 - 30)) /
(CALADC12_12V_85C - CALADC12_12V_30C) + 30.0f;
//print temp value to UART terminal
int temp_int = floor(temperatureDegC);
int temp_rmndr = floor((temperatureDegC - temp_int) * 1000);
ltoa(memval, mv_char, 10);
ltoa(temp_int,temp_int_char, 10);
ltoa(temp_rmndr,temp_rm_char, 10);
ser_output(charmemval); ser_output(mv_char); ser_output(newline);
ser_output(temperature); ser_output(temp_int_char); ser_output(dot); ser_output(temp_rm_char); ser_output(newline);
// P1OUT &= ~BIT2; // stop driving pmos source
// P1OUT |= BIT4; //PMOS gate high to disconnect from the circuit
P1OUT |= BIT0; // set pin 1.0 as high indicating completion of zigbee communication
while(1)
{
__no_operation();
//for(i=0; i<30000;i++){}
// Temperature in Fahrenheit Tf = (9/5)*Tc + 32
//temperatureDegF = temperatureDegC * 9.0f / 5.0f + 32.0f;
// __no_operation(); // SET BREAKPOINT HERE
}
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=ADC12_VECTOR
__interrupt void ADC12ISR (void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC12_VECTOR))) ADC12ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(ADC12IV, ADC12IV_ADC12RDYIFG))
{
case ADC12IV_NONE: break; // Vector 0: No interrupt
case ADC12IV_ADC12OVIFG: break; // Vector 2: ADC12MEMx Overflow
case ADC12IV_ADC12TOVIFG: break; // Vector 4: Conversion time overflow
case ADC12IV_ADC12HIIFG: break; // Vector 6: ADC12BHI
case ADC12IV_ADC12LOIFG: break; // Vector 8: ADC12BLO
case ADC12IV_ADC12INIFG: break; // Vector 10: ADC12BIN
case ADC12IV_ADC12IFG0: // Vector 12: ADC12MEM0 Interrupt
temp = ADC12MEM0; // Move results, IFG is cleared
__bic_SR_register_on_exit(LPM0_bits); // Exit active CPU
break;
case ADC12IV_ADC12IFG1: break; // Vector 14: ADC12MEM1
case ADC12IV_ADC12IFG2: break; // Vector 16: ADC12MEM2
case ADC12IV_ADC12IFG3: break; // Vector 18: ADC12MEM3
case ADC12IV_ADC12IFG4: break; // Vector 20: ADC12MEM4
case ADC12IV_ADC12IFG5: break; // Vector 22: ADC12MEM5
case ADC12IV_ADC12IFG6: break; // Vector 24: ADC12MEM6
case ADC12IV_ADC12IFG7: break; // Vector 26: ADC12MEM7
case ADC12IV_ADC12IFG8: break; // Vector 28: ADC12MEM8
case ADC12IV_ADC12IFG9: break; // Vector 30: ADC12MEM9
case ADC12IV_ADC12IFG10: break; // Vector 32: ADC12MEM10
case ADC12IV_ADC12IFG11: break; // Vector 34: ADC12MEM11
case ADC12IV_ADC12IFG12: break; // Vector 36: ADC12MEM12
case ADC12IV_ADC12IFG13: break; // Vector 38: ADC12MEM13
case ADC12IV_ADC12IFG14: break; // Vector 40: ADC12MEM14
case ADC12IV_ADC12IFG15: break; // Vector 42: ADC12MEM15
case ADC12IV_ADC12IFG16: break; // Vector 44: ADC12MEM16
case ADC12IV_ADC12IFG17: break; // Vector 46: ADC12MEM17
case ADC12IV_ADC12IFG18: break; // Vector 48: ADC12MEM18
case ADC12IV_ADC12IFG19: break; // Vector 50: ADC12MEM19
case ADC12IV_ADC12IFG20: break; // Vector 52: ADC12MEM20
case ADC12IV_ADC12IFG21: break; // Vector 54: ADC12MEM21
case ADC12IV_ADC12IFG22: break; // Vector 56: ADC12MEM22
case ADC12IV_ADC12IFG23: break; // Vector 58: ADC12MEM23
case ADC12IV_ADC12IFG24: break; // Vector 60: ADC12MEM24
case ADC12IV_ADC12IFG25: break; // Vector 62: ADC12MEM25
case ADC12IV_ADC12IFG26: break; // Vector 64: ADC12MEM26
case ADC12IV_ADC12IFG27: break; // Vector 66: ADC12MEM27
case ADC12IV_ADC12IFG28: break; // Vector 68: ADC12MEM28
case ADC12IV_ADC12IFG29: break; // Vector 70: ADC12MEM29
case ADC12IV_ADC12IFG30: break; // Vector 72: ADC12MEM30
case ADC12IV_ADC12IFG31: break; // Vector 74: ADC12MEM31
case ADC12IV_ADC12RDYIFG: break; // Vector 76: ADC12RDY
default: break;
}
}
void ser_output(char *str){
while(*str != 0){
while (!(UCA0IFG&UCTXIFG));
UCA0TXBUF = *str++;
}
}
void initialize_UART(void)
{
// Configure GPIO
P2SEL1 |= BIT0 | BIT1; // USCI_A0 UART operation
P2SEL0 &= ~(BIT0 | BIT1);
//P4DIR |= BIT6;
//P4OUT &= ~BIT6;
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Startup clock system with max DCO setting ~8MHz
CSCTL0_H = CSKEY >> 8; // Unlock clock registers
CSCTL1 = DCOFSEL_3 | DCORSEL; // Set DCO to 8MHz
CSCTL2 = SELA__VLOCLK | SELS__DCOCLK | SELM__DCOCLK;
CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers
CSCTL0_H = 0; // Lock CS registers
// Configure USCI_A0 for UART mode
UCA0CTLW0 = UCSWRST; // Put eUSCI in reset
UCA0CTLW0 |= UCSSEL__SMCLK; // CLK = SMCLK
// Baud Rate calculation
// 8000000/(16*9600) = 52.083
// Fractional portion = 0.083
// User's Guide Table 21-4: UCBRSx = 0x04
// UCBRFx = int ( (52.083-52)*16) = 1
UCA0BR0 = 52; // 8000000/16/9600
UCA0BR1 = 0x00;
UCA0MCTLW |= UCOS16 | UCBRF_1;
UCA0CTLW0 &= ~UCSWRST;
// UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
}
Thanks in advance.