Part Number: MSP430I2040
Other Parts Discussed in Thread: UNIFLASH,
Hello Folks,
Currently programming of and metering with the EVM is done.
Presently i wanted to burn the code only to IC where various required pin connection is made out i.e. 3.3V, GND, TCK and TDIO for flashing the code whereas RXD,TXD along with 3.3V,GND for metering are carried outside.
Now for flashing code i did,
1. Connection of daughter board having IC with HID bridge is done.
2. Same code of EVM430i2040s(Pre-stored) selected in Uniflash for flashing.
3. Error occurring - Cannot read property 'DS' of undefined.
So what should be done for flashing code successfully to IC only, also please advise which things have to be considered while metering.
BR
Gautam