Part Number: MSP430FG6626
Other Parts Discussed in Thread: UNIFLASH, MSP-FET
Hi,
I'm using MSP430FG6626 MCU.
Attached schematics which I have captured from the reference document SLAU278AH.
For detailing the schematics I used page 169 of document SLAU278AH.
I power up the board and connected the USB port to system/laptop.
Tried connecting it using UniFlash tool. I was under the assumption that MSP430FG6626 comes with boot loader and by MCU_SCH.pdfdirectly connecting the USB tool we can program the IC.
When I connect using UniFlash tool the target is not recognized.
Error I get is " "Fatal Error:Could not find device " Error in MSP-FET and MSP430"
Could you please confirm if I need to procure "MSP-FET" MCU Programmer & Debugger ?
Does MSP430FG6626 can be programmed directly without MSP-FET Programmer? Please clarify
Thanks,
Phani