This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430F5529: MSP-EXP430F5529

Part Number: MSP-EXP430F5529

Following the instructions from the online manual of MSP-EXP430F5529 (section 3.2), I downloaded and install the required software and the latest code examples MSP-EXP430F5529_UE_1_31_00_00. I then proceeded to section 3.3 - Working With the Example Software and got the imported error in step #5. Did I import CCS7.2 project into CCS10 by doing above steps - instructed by the manual? Do you mean the project in EXP430F5529_UE_1_31_00_00 is CCS7.2 version? How do I find out the version of project, and more important, how to I make it work?

  • Hi Hien,

    Can you provide the exact error message? I also followed the instructions in section 3.2 and 3.3 of the User's Guide and was able to successfully import the project in CCS10 as shown in the image below.

    Thanks,

    Urica Wang

**Attention** This is a public forum