Part Number: MSP430F6435
NOTE: 5ppm 32.768K crystal for XT1, the VBAT pin is connected to a 3-V rechargeable coin cell battery.
Issue:
The interference and wiring issues are eliminated, various matching capacitors are tried, and the error is still large. Some are 1-hour errors of about 1 second, and some are 2-hour errors of 1 second.
And the customer has tried the following methods:
1.The accuracy is better if the MCU does not go into the sleep LPM3 state and remains active.
2.Set BAKDIS in BAKCTL to 1 for better accuracy. However, the backup battery cannot be used after the power down.
The customer would like to know if there are better ways to achieve it.
Thanks!
Best Regards,
Cherry Zhou