I have the MSP430 SPI setup to talk to a slave peripheral. The wakeup sequence has a total of 9 transactions. There is a return byte expected after transaction 5. No other transactions returns a byte. I am having trouble with SPI receive. It seems to take on a value of 0xff with every byte and this triggers the receive interrupt. I am not able to complete the sequence successfully because I am not getting back the needed byte. The slaves work fine with the evaluation GUI. I appreciate pointers on what can be changed here.
Going to experiment will a polled approach.
#include <stdio.h>
#include <stdlib.h>
#include <stdint.h>
#include <string.h>
#include <driverlib.h>
#include <msp430.h>
#include "clock~.h" // Clock configurations
static uint8_t TXData = 0; //transaction count
static uint8_t RXData = 0; //SPI receive byte
static uint8_t waitForReceive = 0;
typedef struct {
uint8_t Len;
uint8_t Data[5];
} spi_MaximTrans_t;
static spi_MaximTrans_t DCInit_transactions[15];
uint8_t SPI_TX_index = 0; //byte count in transaction
/**
* Initialize system clocks
*/
static void init_clock(void) {
// Configure one FRAM waitstate as required by the device datasheet for MCLK
// operation beyond 8MHz _before_ configuring the clock system.
FRAMCtl_configureWaitStateControl(FRAMCTL_ACCESS_TIME_CYCLES_1);
//Set DCO FLL reference = REFO
CS_initClockSignal(CS_FLLREF, CS_REFOCLK_SELECT, CS_CLOCK_DIVIDER_1);
//Set ACLK = REFO
CS_initClockSignal(CS_ACLK, CS_REFOCLK_SELECT, CS_CLOCK_DIVIDER_1);
CS_initFLLParam param = {0};
//Set Ratio/Desired MCLK Frequency, initialize DCO, save trim values
CS_initFLLCalculateTrim(CS_MCLK_DESIRED_FREQUENCY_IN_KHZ, CS_MCLK_FLLREF_RATIO, ¶m);
//Set MCLK = REFO
CS_initClockSignal(CS_MCLK, CS_REFOCLK_SELECT, CS_CLOCK_DIVIDER_1);
//Set SMCLK = DCO
CS_initClockSignal(CS_SMCLK, CS_DCOCLKDIV_SELECT, CS_CLOCK_DIVIDER_1);
//Clear all OSC fault flag
CS_clearAllOscFlagsWithTimeout(1000);
}
/**
* Initialize all of the IO pins per their configuration
*/
static void init_gpio(void) {
// Set all GPIO pins to output low to prevent floating input and reduce power consumption
GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN_ALL8);
GPIO_setOutputLowOnPin(GPIO_PORT_P2, GPIO_PIN_ALL8);
GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN_ALL8);
GPIO_setOutputLowOnPin(GPIO_PORT_P4, GPIO_PIN_ALL8);
GPIO_setOutputLowOnPin(GPIO_PORT_P5, GPIO_PIN_ALL8);
GPIO_setOutputLowOnPin(GPIO_PORT_P6, GPIO_PIN0 | GPIO_PIN1 | GPIO_PIN2);
GPIO_setAsOutputPin( GPIO_PORT_P1, GPIO_PIN_ALL8);
GPIO_setAsOutputPin( GPIO_PORT_P2, GPIO_PIN_ALL8);
GPIO_setAsOutputPin( GPIO_PORT_P3, GPIO_PIN_ALL8);
GPIO_setAsOutputPin( GPIO_PORT_P4, GPIO_PIN_ALL8);
GPIO_setAsOutputPin( GPIO_PORT_P5, GPIO_PIN_ALL8);
GPIO_setAsOutputPin( GPIO_PORT_P6, GPIO_PIN0 | GPIO_PIN1 | GPIO_PIN2);
}
/*
* Initialize the SPI peripheral on EUSCI A1
*/
void init_spi_peripheral()
{
//Initialize Master
EUSCI_A_SPI_initMasterParam param = {0};
param.selectClockSource = EUSCI_A_SPI_CLOCKSOURCE_SMCLK;
param.clockSourceFrequency = CS_getSMCLK();
param.desiredSpiClock = 1000000;
param.msbFirst = UCMSB;
param.clockPhase = 0;
param.clockPolarity = EUSCI_A_SPI_CLOCKPOLARITY_INACTIVITY_LOW;
param.spiMode = EUSCI_A_SPI_3PIN;
EUSCI_A_SPI_initMaster(EUSCI_A1_BASE, ¶m);
EUSCI_A_SPI_enable(EUSCI_A1_BASE);
// Enable the TX and RX interrupts for the SPI bus.
EUSCI_A_SPI_enableInterrupt(EUSCI_A1_BASE, EUSCI_A_SPI_TRANSMIT_INTERRUPT);
EUSCI_A_SPI_enableInterrupt(EUSCI_A1_BASE, EUSCI_A_SPI_RECEIVE_INTERRUPT);
}
void SetUpTransactions(void){
//Enable keep alive mode
DCInit_transactions[0].Len = 2;
DCInit_transactions[0].Data[0] = 0x10;
DCInit_transactions[0].Data[1] = 0x5; //No Receive
//Enable Rx Interrupt flags
DCInit_transactions[1].Len = 2;
DCInit_transactions[1].Data[0] = 0x4;
DCInit_transactions[1].Data[1] = 0x88; //No Receive
//Clear receive buffer
DCInit_transactions[2].Len = 1;
DCInit_transactions[2].Data[0] = 0xe0; //No Receive
//Wakeup UART slave devices
DCInit_transactions[3].Len = 2;
DCInit_transactions[3].Data[0] = 0xe0;
DCInit_transactions[3].Data[1] = 0x30; //No Receive
//Wait for all UART slave devices to wake up
DCInit_transactions[4].Len = 1;
DCInit_transactions[4].Data[0] = 0x01; //Receive of 0x21 expected
//End of UART slave device wake-up period
DCInit_transactions[5].Len = 2;
DCInit_transactions[5].Data[0] = 0x0e;
DCInit_transactions[5].Data[1] = 0x10; //No Receive
//Wait for null message to be received
DCInit_transactions[6].Len = 1;
DCInit_transactions[6].Data[0] = 0x01; //No Receive
//Clear transmit buffer
DCInit_transactions[7].Len = 1;
DCInit_transactions[7].Data[0] = 0x20; //No Receive
//Clear receive buffer
DCInit_transactions[8].Len = 1;
DCInit_transactions[8].Data[0] = 0xe0; //No Receive
}
/**
* main.c
*/
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer
init_clock();
init_gpio(); // Set up IO pins
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN1);
// Configure SPI Pins for UCA1CLK, UCA1TXD/UCA1SIMO and UCA1RXD/UCA1SOMI
/*
* Select Port 2
* Set Pin 4, Pin 5 and Pin 6 to input Secondary Module Function
*/
GPIO_setAsPeripheralModuleFunctionInputPin(
GPIO_PORT_P2,
GPIO_PIN4 + GPIO_PIN5 + GPIO_PIN6,
GPIO_PRIMARY_MODULE_FUNCTION
);
// Set P1.0 to output direction
GPIO_setAsOutputPin (GPIO_PORT_P1, GPIO_PIN0);
GPIO_setAsInputPinWithPullUpResistor (GPIO_PORT_P4, GPIO_PIN2);
GPIO_enableInterrupt (GPIO_PORT_P4, GPIO_PIN2);
GPIO_selectInterruptEdge (GPIO_PORT_P4, GPIO_PIN2, GPIO_HIGH_TO_LOW_TRANSITION);
GPIO_clearInterrupt (GPIO_PORT_P4, GPIO_PIN2);
PMM_unlockLPM5();
SetUpTransactions();
TXData = 0x0; // Holds transaction number
// Setup peripheral(s) now that gpio and clocks are setup
init_spi_peripheral(); // Init Maxim spi peripheral
//Wait for slave to initialize
__delay_cycles(100);
GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN1); //Maxim chip select low
UCA1IFG |= UCTXIFG;
__bis_SR_register(LPM0_bits + GIE); // CPU off, enable interrupts
__no_operation(); // Remain in LPM0
return 0;
}
//******************************************************************************
//
//This is the PORT2_VECTOR interrupt vector service routine
//
//******************************************************************************
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=PORT4_VECTOR
__interrupt
#elif defined(__GNUC__)
__attribute__((interrupt(PORT2_VECTOR)))
#endif
void P4_ISR (void)
{
// GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN1);
GPIO_clearInterrupt (GPIO_PORT_P4, GPIO_PIN2);
// Toggle P1.0 output
GPIO_toggleOutputOnPin (GPIO_PORT_P1, GPIO_PIN0);
GPIO_disableInterrupt (GPIO_PORT_P4, GPIO_PIN2);
}
/****************************************************************************
* EUSCI_A1_isr()
*
* This interrupt is used for SPI interrupts (UCA1).
****************************************************************************/
#pragma vector = EUSCI_A1_VECTOR
__interrupt void EUSCI_A1_isr(void)
{
// SPI TX interrupt?
if (UCA1IFG & UCTXIFG)
{
while (UCA1STATW & UCBUSY);
EUSCI_A_SPI_transmitData(EUSCI_A1_BASE, DCInit_transactions[TXData].Data[SPI_TX_index]);
SPI_TX_index++;
if (SPI_TX_index == DCInit_transactions[TXData].Len){
SPI_TX_index = 0;
if (!waitForReceive)
TXData = TXData+1;
if (TXData == 5){
TXData = 4;
waitForReceive = 1;
}
if (TXData == 9) {
while (UCA1STATW & UCBUSY); //wait for the last byte to transmit
EUSCI_A_SPI_disableInterrupt(EUSCI_A1_BASE, EUSCI_A_SPI_TRANSMIT_INTERRUPT);
EUSCI_A_SPI_disableInterrupt(EUSCI_A1_BASE, EUSCI_A_SPI_RECEIVE_INTERRUPT);
}
}
/* Put a new byte to send into the TX buffer.
* This prevents us from stuffing an extra byte.
*****/
/* Disable the TX interrupt. Since the last byte of the message
* has been sent, disable the TX interrupt. If this is not done,
* the ISR will be repeatedly invoked between the time that the
* time that the UCA1TXBUF is empty and the time that the receive
* byte is available in UCA1RXBUF.
*****/
}
if (UCA1IFG & UCRXIFG)
{
RXData = EUSCI_A_SPI_receiveData(EUSCI_A1_BASE);
if (waitForReceive && (RXData == 0x21)){
waitForReceive = 0;
TXData = 5;
}
}
}