Part Number: MSP430FR2355
Hello,
I would like to use IQ or QMathLib with MSP430FR2355 and take advantage of the MPY32 multiplier. I do not see support in the IQMathLib for the MSP430FR2355 and MPY32 specifically. I can manually add support for it myself but it would be better to use a ready made library.
How can I add the IQMathLib to the CCS 10.4.0.00006 so that the library is using the MPY32 peripheral? How do I set it in the project properties?
Thank you
Sagi