This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2675: FW compatible

Part Number: MSP430FR2675

Can the firmware image created on one orderable be shared between all of the orderable devices that share the same datasheet with  MSP430FR2675TPT without changing it?

  • Hi TJ,

    It depends.  In general, yes, but the customer should review the datasheet for both devices and ensure the memory, peripherals and IO used in the FR2675 image exist on the other device.  For example, the FR2675 has FRAM starting at 8000h, but the FR2673 starts at C000h.  So if the FR2675 compiled image places the start of code at 8000h, this memory range does not exist on FR2673.  But look at FR2676.  It does have starting address so FR2676 and FR2675 could potentially share the image.

    Does this help?

  • Hi TJ,

    I haven't heard back from you so I'll assume your question was answered.
    If this isn’t the case, please click the "This did NOT resolve my issue" button and reply to this thread with more information.
    If this thread locks, please click the "Ask a related question" button and in the new thread describe the current status of your issue and any additional details you may have to assist us in helping to solve your issues.

  • Sorry for the slow reply Dennis. Your message was exactly what i needed confirmed. Thanks for the help and have a good week!

**Attention** This is a public forum