Hello Everyone,
I am trying to build a clamp on flow meter using MSP430FR6047 and Jiakang 1-MHz Transducer, I made a test setup as shown below. I am using a 50 mm pipe and set the parameters as shown below.
When I am pumping water through it at 500 L/H I get the following graphs.
Can some one please explain why my Delta TOF have negative values, also flow rate is having negative values in the graph. Is this normal or something wrong with my configuration?
Also how can I display the real time flow rate in MSP LCD?
Please help, thanks in advance.