This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sensors....

Hi,

I am trying to read temperature and pressure from Bosch BMP085 device. I have writtern a code ( given below) but the problem is that I can not get right values for both temperature and pressure.

My problems are that when I calibarate data ( using step into fuction) I am not receiving expected values of register. Could anyone look  into my code and advice me what is wrong with the code.

 It also kept receiving the value and save in the RXbuffer, even though I dont want to.

 

#include

 

"msp430x22x4.h"

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

//#define NUM_BYTES_TX 1 // How many bytes?

//#define NUM_BYTES_RX 24 // Set to two to read one byte from the slave

volatile

 

 

unsigned char NUM_BYTES_TX = 1;

// How many bytes?

volatile

 

 

unsigned char NUM_BYTES_RX = 24;

// Set to two to read one byte from the slave

int

 

 

RXByteCtr, RPT_Flag = 0;

// enables repeated start when 1

volatile

 

 

unsigned char RxBuffer[24];

// Allocate 24 byte of RAM

volatile

 

 

unsigned char RxBufferIndex = 0;

// Sets the location where the received data is stored

unsigned

 

 

char *PTxData;

// Pointer to TX data

unsigned

 

 

char *PRxData;

// Pointer to RX data

unsigned

 

 

char

TXByteCtr, RX = 0;

unsigned

 

 

char

MSData = 0xAA;

unsigned

 

 

char

address = 0;

unsigned

 

 

char

data = 0;

const

 

 

unsigned char oversampling_setting=3;

// oversampling for measurement

const

 

 

unsigned char pressure_converstiontime[4]= {0,1,2,3} ;

// delays for oversampling settings 0,1,2 and 3

 

//unsigned char UTdata = 0x2E;

 

 

// sensor registers from BOSCH BMP085

 

 

 

short

ac1=0;

 

 

short

ac2=0;

 

 

short

ac3=0;

 

 

unsigned short

ac4=0;

 

 

unsigned short

ac5=0;

 

 

unsigned short

ac6=0;

 

 

short

b1=0;

 

 

short

b2=0;

 

 

short

mb=0;

 

 

short

mc=0;

 

 

short

md=0;

 

 

// Variable to keep the values

 

 

 

int

temperature = 0;

 

 

long

pressure = 0;

 

// Prototypes

void

 

 

Setup_TX(void

);

void

 

 

Setup_RX(void

);

void

 

 

Transmit(void

);

void

 

 

Receive(void

);

void

 

 

calibraitonData(void

);

void

 

 

writeRegister(unsigned char address, unsigned char

data);

int

 

 

readIntRegister(unsigned char

address);

unsigned

 

 

char readRegister(unsigned char

address);

unsigned

 

 

int

readUT();

long

 

 

readUP();

void

 

 

readSensor();

void

 

 

main(void

)

{

WDTCTL = WDTPW + WDTHOLD;

 

// Stop WDT

P3SEL |= 0x06;

 

// Assign I2C pins to USCI_B0

 

 

 

//while(1)

 

 

// {

 

calibraitonData();

 

 

//writeRegister(address, data);

 

 

//readIntRegister(address);

 

 

// readRegister(address);

// readIntRegister(UT);

readSensor();

 

 

 

//}

}

//-------------------------------------------------------------------------------

// The USCI_B0 data ISR is used to move received data from the I2C slave

// to the MSP430 memory. It is structured such that it can be used to receive

// any 2+ number of bytes by pre-loading RXByteCtr with the byte count.

//-------------------------------------------------------------------------------

#pragma

 

 

vector = USCIAB0TX_VECTOR

__interrupt

 

void USCIAB0TX_ISR(void

)

{

 

 

if(RX == 1){

// Master Recieve?

RXByteCtr--;

 

// Decrement RX byte counter

 

 

if

(RXByteCtr)

{

*PRxData++ = UCB0RXBUF;

 

// Move RX data to address PRxData

}

 

 

else

{

 

 

if

(RPT_Flag == 0)

UCB0CTL1 |= UCTXSTP;

 

// No Repeated Start: stop condition

 

 

if(RPT_Flag == 1){

// if Repeated Start: do nothing

RPT_Flag = 0;

}

*PRxData = UCB0RXBUF;

 

// Move final RX data to PRxData

__bic_SR_register_on_exit(CPUOFF);

 

// Exit LPM0

}}

 

 

 

else{

// Master Transmit

 

 

if (TXByteCtr)

// Check TX byte counter

{

UCB0TXBUF = MSData++;

 

// Load TX buffer

TXByteCtr--;

 

// Decrement TX byte counter

}

 

 

else

{

 

 

if

(RPT_Flag == 1){

RPT_Flag = 0;

PTxData = &MSData;

 

// TX array start address

TXByteCtr = NUM_BYTES_TX;

 

// Load TX byte counter

__bic_SR_register_on_exit(CPUOFF);

}

 

 

else

{

UCB0CTL1 |= UCTXSTP;

 

// I2C stop condition

IFG2 &= ~UCB0TXIFG;

 

// Clear USCI_B0 TX int flag

__bic_SR_register_on_exit(CPUOFF);

 

// Exit LPM0

}

}

}

 

}

void

 

 

Setup_TX(void

){

_DINT();

RX = 0;

IE2 &= ~UCB0RXIE;

 

 

while (UCB0CTL1 & UCTXSTP);

// Ensure stop condition got sent// Disable RX interrupt

UCB0CTL1 |= UCSWRST;

 

// Enable SW reset

UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC;

 

// I2C Master, synchronous mode

UCB0CTL1 = UCSSEL_2 + UCSWRST;

 

// Use SMCLK, keep SW reset

UCB0BR0 = 12;

 

// fSCL = SMCLK/12 = ~100kHz

UCB0BR1 = 0;

UCB0I2CSA = 0x77;

 

// Slave Address is 048h

UCB0CTL1 &= ~UCSWRST;

 

// Clear SW reset, resume operation

IE2 |= UCB0TXIE;

 

// Enable TX interrupt

}

void

 

 

Setup_RX(void

){

_DINT();

RX = 1;

IE2 &= ~UCB0TXIE;

UCB0CTL1 |= UCSWRST;

 

// Enable SW reset

UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC;

 

// I2C Master, synchronous mode

UCB0CTL1 = UCSSEL_2 + UCSWRST;

 

// Use SMCLK, keep SW reset

UCB0BR0 = 12;

 

// fSCL = SMCLK/12 = ~100kHz

UCB0BR1 = 0;

UCB0I2CSA = 0x77;

 

// Slave Address is 048h

UCB0CTL1 &= ~UCSWRST;

 

// Clear SW reset, resume operation

IE2 |= UCB0RXIE;

 

// Enable RX interrupt

}

void

 

 

Transmit(void

){

PTxData = &MSData;

 

// TX array start address

TXByteCtr = NUM_BYTES_TX;

 

// Load TX byte counter

 

 

while (UCB0CTL1 & UCTXSTP);

// Ensure stop condition got sent

UCB0CTL1 |= UCTR + UCTXSTT;

 

// I2C TX, start condition

__bis_SR_register(CPUOFF + GIE);

 

// Enter LPM0 w/ interrupts

}

void

 

 

Receive(void

){

PRxData = (

 

unsigned char *)RxBuffer;

// Start of RX buffer

RXByteCtr = NUM_BYTES_RX-1;

 

// Load RX byte counter

 

 

while (UCB0CTL1 & UCTXSTP);

// Ensure stop condition got sent

UCB0CTL1 |= UCTXSTT;

 

// I2C start condition

__bis_SR_register(CPUOFF + GIE);

 

// Enter LPM0 w/ interrupts

}

 

// get calibration data.....

void

 

 

calibraitonData(void

)

{

 

 

 

//Transmit process

Setup_TX();

RPT_Flag = 0;

Transmit();

 

 

while (UCB0CTL1 & UCTXSTP);

// Ensure stop condition got sent

 

 

 

//Receive process

Setup_RX();

Receive();

 

 

while (UCB0CTL1 & UCTXSTP);

// Ensure stop condition got sent

 

ac1 = (

 

short

) RxBuffer[0]<<8 | RxBuffer[1];

ac2 = (

 

short

) RxBuffer[2]<<8 | RxBuffer[3];

ac3 = (

 

short

) RxBuffer[4]<<8 | RxBuffer[5];

ac4 = (

 

unsigned short

) RxBuffer[6]<<8 | RxBuffer[7];

ac5 = (

 

unsigned short

) RxBuffer[8]<<8 | RxBuffer[9];

ac6 = (

 

unsigned short

) RxBuffer[10]<<8 | RxBuffer[11];

b1 = (

 

short

) RxBuffer[12]<<8 | RxBuffer[13];

b2 = (

 

short

) RxBuffer[14]<<8 | RxBuffer[15];

mb = (

 

short

) RxBuffer[16]<<8 | RxBuffer[17];

mc = (

 

short

) RxBuffer[18]<<8 | RxBuffer[19];

md = (

 

short

) RxBuffer[20]<<8 | RxBuffer[21];

}

 

// write 0x2E into reg 0xF4, wait 4.5ms

void

 

 

writeRegister(unsigned char address, unsigned char

data)

{

 

NUM_BYTES_TX = 1;

MSData = address;

 

Setup_TX();

RPT_Flag = 0;

Transmit();

 

 

while

(UCB0CTL1 & UCTXSTP);

 

MSData = data;

 

Setup_TX();

RPT_Flag = 0;

Transmit();

 

 

while

(UCB0CTL1 & UCTXSTP);

}

 

 

// read register 0xF6 (MSB) , 0xF7 (LSB) ---> 16 bit

int

 

 

readIntRegister(unsigned char

address)

{

NUM_BYTES_RX = 5;

MSData = address;

 

Setup_TX();

RPT_Flag = 0;

Transmit();

 

 

while

(UCB0CTL1 & UCTXSTP);

 

Setup_RX();

Receive();

 

 

while

(UCB0CTL1 & UCTXSTP);

 

 

 

return (RxBuffer[0]) <<8 | (int

)(RxBuffer[1]);

}

//

// read an 8 bit register

unsigned

 

 

char readRegister(unsigned char

address)

{

NUM_BYTES_RX= 5;

MSData = address;

 

Setup_TX();

RPT_Flag = 0;

Transmit();

 

 

while

(UCB0CTL1 & UCTXSTP);

 

Setup_RX();

Receive();

 

 

while

(UCB0CTL1 & UCTXSTP);

 

 

return

RxBuffer[0];

}

 

// read uncompensated temperature value

unsigned

 

 

int

readUT()

{

writeRegister(0xF4,0x2E);

__delay_cycles(54022);

 

// wait of 4.5ms

 

 

return

readIntRegister(0xF6);

 

}

 

// read uncompensated pressure value

long

 

 

readUP()

{

writeRegister(0xF4,0x34+(oversampling_setting<<6));

 

 

//_delay_cycles(pressure_converstiontime[oversampling_setting]);

 

NUM_BYTES_RX = 5;

MSData = address;

 

Setup_TX();

RPT_Flag = 0;

Transmit();

 

 

while

(UCB0CTL1 & UCTXSTP);

 

Setup_RX();

Receive();

 

 

while

(UCB0CTL1 & UCTXSTP);

 

 

 

//return (RxBuffer[0]) <<8 | (int)(RxBuffer[1]);

 

 

return (((long)RxBuffer[0] <<16) | ((long)RxBuffer[1]<<8) | ((long

)RxBuffer[2])) >> (8-oversampling_setting);

 

 

// unsigned char *msb,*lsb,*xlsb;

// Setup_TX();

// unsigned char address = 0xF6;

// Transmit();

//

// Setup_RX();

// msb = PRxData;

// Receive();

// lsb = PRxData;

// Receive();

// xlsb = PRxData;

// Receive();

//

// return (((long)msb<<16) | ((long)lsb<<8) | ((long)xlsb)) >> (8-oversampling_setting);

 

}

 

 

 

// utility functions to get data from the sensor

 

// read temperature and pressure from sensor

void

 

 

readSensor()

{

 

 

long

ut=readUT();

 

 

long

up = readUP();

 

 

long

x1,x2,x3,b3,b5,b6,p;

 

 

unsigned long

b4,b7;

 

 

 

//calculate true temperature

x1 = ((

 

long

)ut - ac6) * ac5 >> 15;

x2 = ((

 

long

) mc << 11) / (x1 + md);

b5 = x1 + x2;

temperature = (b5 + 8) >> 4;

 

 

 

//calculate true pressure

b6 = b5 - 4000;

x1 = (b2 * (b6 * b6 >> 12)) >> 11;

x2 = ac2 * b6 >> 11;

x3 = x1 + x2;

b3 = ((ac1 * 4 + x3)<<oversampling_setting + 2) >> 2;

x1 = ac3 * b6 >> 13;

x2 = (b1 * (b6 * b6 >> 12)) >> 16;

x3 = ((x1 + x2) + 2) >> 2;

b4 = (ac4 * (

 

unsigned long

) (x3 + 32768)) >> 15;

b7 = ((

 

unsigned long

) up - b3) * (50000 >> oversampling_setting);

**Attention** This is a public forum