This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5733: Internal resistance values of P1.0 and P1.3

Part Number: MSP430FR5733

Hi experts,

My customer wants to know the difference between the internal resistance values of P1.0 and P1.3.
They measured the internal resistance values of P1.0 and P1.3 when the MSP430 was powered off.
As a result, P1.0 was 24kΩ and P1.3 was 2.4kΩ.

Can you explain the difference between the internal resistance values of P1.0 and P1.3?
If the information is not publicly available, I will tell the customer that it is not publicly available.

Best regards,
Sasaki

**Attention** This is a public forum