Part Number: MSP430F67641A
Other Parts Discussed in Thread: MSP430F67641
Dear Team,
I am interfacing an RF module through Asynchronous UART at 9600 baudrate. My RF module is receiving data every 2 seconds once and writing out to be read by the controller MSP430F67641.
The problem i face is that, whenever i place a breakpoint in my code, i get an overrun error set (UCOE and UCRXERR set) and i am no longer able to receive any data anymore until i hit a full reset.
I do not get this issue while i do not halt the target with breakpoints and allow it to run continuously. I know that if i halt the core with a breakpoint, the external RF still receives some data and writes the data to the controller and there is surely some data missed to be received. But i expected that UART module is also be paused without receiving anything and just the intermediate data is lost instead of a overrun error.
I did not notice this strange overrun behaviour in the other MSP430 controllers i used in other projects while in breakpoint.
Attached the key parts of my code. Could you please help here ?
Thanks
Surya
void SetClock_24Mhz()
{
SetVCore(3);
// Setup UCS
UCSCTL3 |= SELREF_2; // Set DCO FLL reference = REFO
UCSCTL4 |= SELA_2; // Set ACLK = REFO
UCSCTL5 |= DIVS__2 | DIVA__4 | DIVM__1;
UCSCTL4 |= SELM__REFOCLK | SELS__REFOCLK | SELA__REFOCLK; /* 24MHz MCLK, 12MHz SMCLK, ACLK (6Mhz)*/
__bis_SR_register(SCG0); // Disable the FLL control loop
UCSCTL0 = 0x0000; // Set lowest possible DCOx, MODx
UCSCTL1 = DCORSEL_7; // Select DCO range 24MHz operation
UCSCTL2 = FLLD_1 | 732; // Set DCO Multiplier for 24MHz
// (N + 1) * FLLRef = Fdco
// (732 + 1) * 32768 = 24MHz
// Set FLL Div = fDCOCLK/2
__bic_SR_register(SCG0); // Enable the FLL control loop
__delay_cycles(250000);
__delay_cycles(250000);
__delay_cycles(250000);
__delay_cycles(250000);
// Loop until XT1, XT2 & DCO fault flag is cleared
do
{
UCSCTL7 &= ~(XT2OFFG | XT1LFOFFG | DCOFFG);
// Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
} while (SFRIFG1 & OFIFG); // Test oscillator fault flag
SFR_clearInterrupt(SFR_OSCILLATOR_FAULT_INTERRUPT);
SFR_enableInterrupt(SFR_OSCILLATOR_FAULT_INTERRUPT);
__delay_cycles(250000);
}
void Uart_Init_9600()
{
// Setup P2.2 UCA2RXD, P2.3 UCA2TXD
P2SEL |= BIT2 | BIT3; // Set P2.2, P2.3 to non-IO
P2DIR |= BIT2 | BIT3; // Enable UCA2RXD, UCA2TXD
// Setup eUSCI_A2
UCA2CTLW0 |= UCSWRST; // **Put state machine in reset**
UCA2CTLW0 |= UCSSEL__SMCLK | UCRXEIE; // SMCLK (12Mhz) accurate -> 12009472 Hz
/*
* Baud Rate calculation (9600) [PAge No- 586 user guide 2433]
* 12009472/(9600) = 1250 [Greater than 16. So proceed with next calc's]
* (1250.987/16) = 78.186 => (UCA1BR0 = 78)
*
* UCBRFx = (0.186*16) = 2.98 => 3 roundoff
* User's Guide Table 22-4: Decimal value of (0.00) is UCBRSx = 0x00
*/
UCA2BRW = 78; // 24MHz 9600
UCA2MCTLW = UCBRF_3 | UCOS16; // Modln UCBRSx=0, UCBRFx=0x13,
UCA2CTLW0 &= ~UCSWRST; // **Initialize USCI state machine**
UCA2IE |= UCRXIE; // Enable USCI_A2 RX interrupt
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A2_VECTOR
__interrupt void USCI_A2_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A2_VECTOR))) USCI_A2_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch (__even_in_range(UCA2IV, USCI_UART_UCTXCPTIFG))
{
case USCI_NONE: break; // No interrupt
case USCI_UART_UCRXIFG: // RXIFG
UCA2_Status = UCA2STATW;
if (UCA2_Status & UCRXERR)
{
// This part of code is hit when i set a breakpoint and some data is receiveid during that time
DummyRX = UCA2RXBUF; // Dummy read to clear out data
UARTErrorCnt++;
}
else
{
UartRxBuff[UartRxCnt] = UCA2RXBUF; // TX -> RXed character
/* Check if new line received and set processing flag */
if(UartRxBuff[UartRxCnt] == 0x0A) { UartRxFlg = true; }
UartRxCnt++;
}
/* If RX buffer exceeds then process and flush garbage data */
if(UartRxCnt >= UartRxBuffMAX)
{
UartRxCnt = UartRxBuffMAX;
UartRxFlg = true;
}
break;
case USCI_UART_UCTXIFG: break; // TXIFG
case USCI_UART_UCSTTIFG: break; // TTIFG
case USCI_UART_UCTXCPTIFG: break; // TXCPTIFG
default: break;
}
}