Hi All,
I need some deep technical support for MSP-430 Gang Programmer.
We currently program MSP-430 F2013 devices in two stage using IAR + MS430FET, one of which is loaded for storing some calibration data into info memory and the other is loaded for the end user. The two program cant not be loaded together as the flash space is not enough for such an application. One of the important point here is we need to retain data that we store at info memory in first stage while the msp-430 is being programmed in the second stage. Another important thing is we also need to store some program code into info memory in the second stage of programming. We can do this using IAR with the option Retain Unchanged Memory.
Recently, we decided to move MSP-430 Gang since the IAR and MSP-430 FET is not for mass production purpose, and have bought one.
After we examined the product, we realized that the GANG does not have such an option( Retain Unchanged Memory)?
Can we do what we have doing with IAR + MS430FET by MSP430GANG?
We are in urgent need of finding a solution to this problem.
Best Regards,
Koksal