Part Number: MSP-EXP430G2ET
Other Parts Discussed in Thread: ENERGYTRACE
Good Morning,
we'd like to use MSP-EXP430G2ET to measure our device mean-current consumption using Energy Trace Technology.
The application loop under analysis is quite simple:
5 seconds of deep sleep + ~6ms of execution
During the 6ms of execution the product performs some measurements and a task that require one session of (~40x 4us load spike, one spike every ~60us).
Task Loop in time
_4us _ _4us _ _4us _ spike
___6ms___ / \_60us__/ \__60us_.x20../ \ active
_______5s_____/ \ deep-sleep
From an expected current consumption point of view (T rise/fall ~1us)
_60mA_ _60mA_ _60mA_ spike
___1mA___ / \_1mA__/ \__1mA_.x20../ \ active
______100nA___/ \ deep-sleep
At the moment performed measurements don't match our expectations.
Some further details:
all MSP-EXP430G2ET Jumpers are disconnected.
the device is directly supplied from the MSP-EXP430G2ET GND and 3V3 Pins
a 47uF capacitor is installed in parallel to the device load
We have verified and taken into account that the MSP-EXP430G2ET cannot measures down to 100nA
Taking into account all these pre-conditions the current consumption is still higher the what we'd expect.
So all these considerations lead to our questions:
Before proceeding with further investigations on our side, we would like to know
1. how much we can relay on MSP-EXP430G2ET Energy trace capability to measure the current consumption in our specific application?
2. is it capable to measure such short in time current excursions (1mA->60mA->100nA)?
Thank you very much for your support.
Kind Regards,
Demetrio Pitasi