Other Parts Discussed in Thread: MSP-GANG
Hi team,
The following problem occurs when saving the testcode from the following software interface to the image 1.0 with "Save to Image", and shows the shows the following error: ERROR352.
It's not actually stored in Programr. (Customer can save to Image by doing the same on a previously purchased programr. The problem may is not related to the upper-bit interface and the testcode). Also, the Interactive mode allows to be burned to the target MCU, but can't download the TXT file into MSP GANG PROGRAMMER.


Could you help check this case? Thanks.
Best Regards,
Cherry