Other Parts Discussed in Thread: TEST2
Hello,
i used for 250kbaud this rx rfsetting: (it works perfect)
0x06, // FSCTRL1 Frequency synthesizer control.
0x00, // FSCTRL0 Frequency synthesizer control.
0x23, // FREQ2 Frequency control word, high byte.
0x31, // FREQ1 Frequency control word, middle byte.
0x3B, // FREQ0 Frequency control word, low byte.
0xCA, // MDMCFG4 Modem configuration.
0x83, // MDMCFG3 Modem configuration.
0x10, // MDMCFG2 Modem configuration.
0x22, // MDMCFG1 Modem configuration.
0xF8, // MDMCFG0 Modem configuration.
0x00, // CHANNR Channel number.
0x34, // DEVIATN Modem deviation setting (when FSK modulation is enabled).
0x56, // FREND1 Front end RX configuration.
0x10, // FREND0 Front end TX configuration.
0x18, // MCSM0 Main Radio Control State Machine configuration.
0x16, // FOCCFG Frequency Offset Compensation Configuration.
0x6C, // BSCFG Bit synchronization Configuration.
0x43, // AGCCTRL2 AGC control.
0x40, // AGCCTRL1 AGC control.
0x91, // AGCCTRL0 AGC control.
0xE9, // FSCAL3 Frequency synthesizer calibration.
0x2A, // FSCAL2 Frequency synthesizer calibration.
0x00, // FSCAL1 Frequency synthesizer calibration.
0x1F, // FSCAL0 Frequency synthesizer calibration.
0x59, // FSTEST Frequency synthesizer calibration.
0x81, // TEST2 Various test settings.
0x35, // TEST1 Various test settings.
0x09, // TEST0 Various test settings.
0x47, // FIFOTHR RXFIFO and TXFIFO thresholds.
0x0B, // IOCFG2 GDO2 output pin configuration.
0x0C, // IOCFG0D GDO0 output pin configuration. Refer to SmartRF® Studio User Manual for detailed pseudo register explanation.
0x04, // PKTCTRL1 Packet automation control.
0x12, // PKTCTRL0 Packet automation control.
0x00, // ADDR Device address.
0xFF // PKTLEN Packet length.
Now i will transfer the data synchronously with 500kbaud. If i change the baudrate (500kBaud) an the Rx filter Bw (812KHz) in the smart rfstudio. The RF studio says: Ii should only change the register MDMCFG4=0E. But then the data transmission is very bad.
What should i change? Where can i find some information about the rfsetting for the 500kbaud transmission?