Hello,
Can anyone PLEASE help me out on the simple peer to peer application supplied with the simpliciTI.
I was able to burn the program into both the target boards(Link to and Link listen) using the IAR IDE.
I then followed the steps to set-up the peer to peer connection from the sample applications users guide.
After downloading the program into the target boards, the two LEDs light up on both the boards (as mentioned in the users guide),
I then press the push button on the listener to initiate LinkListen. After this, only the red LED switches-ON on the listner. (This is again as mentioned in the users guide)
I then press the push button on the linkTo target board (where it is SUPPOSED to establish a link with the listener and periodically send and receive 2 byte messages). But, the link does not establish and both the LEDs on the LinkTo device starts blinking thereby indicating that the link was unsuccessful.
I REALLY need help on how to go about this problem so that I can build a chat application as my final project which is due by the end of the next week.
I would greatly appreciate your valuable inputs.
Thanks,
Jim