Part Number: MSP430FR2433
Other Parts Discussed in Thread: MSP-EXP430FR2433, , MSP430FR2355
I have an application where I need to start the controller and establish a UART connection as quickly as possible (temp. range -25°C - +65°C).
Since the FLL needs max. 280ms to lock in and is not very precise, I want to use an external crystal oscillator with 16 MHz on the XT1IN pin (XT1BYPASS mode).
Is this possible? I can't really figure it out from the data sheet.