This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI,
The serial driver for the application side of the UART seems to be buffering characters. I can see characters go out the MSP430FR2433 (pin 1.4) on the scope, but they don't appear in TeraTerm for like 5 seconds later when presumably some timeout on that side occurs. I have seen it work properly a few times, but I don't seem to have any control over this behavior. Is this a bug that got fixed in a later version of CC? I'm using 11.0.0.0012 and Windows 10.
Thanks,
Brett
Ok, I think I see what's going on. When the debugger is running the application UART doesn't respond right away, but when the debugger is not running the response is immediate.
**Attention** This is a public forum