Part Number: MSP430FG6626
Hi,
I have two questions about the MSP430FG6626.
1. UART & LCD
the MSP430FG6626 support 2ch UART, but these are shared with LCD port.
(Yellow is uart port, green is lcd port)
P8.3/UCA1RXD/UCA1SOMI/S12
P8.2/UCA1TXD/UCA1SIMO/S13
P2.4/P2MAP4/R03
P2.5/P2MAP5
My customer's product need to use both UART and LCD.
What is the pin mapping method that can use UART 2ch and LCD simultaneously?
2. DAC
My customer's product also need to use ADC and DAC.
ADC and DAC share a pin.
Can I use the pin shared with the PM for DAC use?
I am going to suggest using P5.1/A4/DAC0, P5.6/A5/DAC1 pins for ADC and P2.1/P2MAP1/DAC1, P2.0/P2MAP0/DAC0 for DAC.
Is there any problem?

And what do pm.y and pm.z mean in DAC?