Part Number: CCSTUDIO-MSP
Hi team,
When running the CCS 11.0.00012 installer, the MSP430 or MSP432 components cannot be installed and an error is reported, then exit. The error message is as follows:
CCS_ERROR: Unable to install repotype executable
D:\ti\ccs1100\ccs\eclipse\downloads\ti_msp430pack_setup64_11.0.0.exe: Error running
D:\ti\ccs1100\ccs\eclipse\downloadsiti_msp430pack_setup64_11.0.0.exe --prefix "D:\ticcs1100/ccs" --eclipseprefix "D:/ti/ccs1100/ccs/eclipse"--mode unattended --installer-log
"D:\ti\ccs1100/ccs/install_logs/20211206144329" --ccs true: child killed:unknown signal.
Do you want to retry?

There has been an error.Error running
D:\ti\ccs1100\ccs\eclipse\downloadsiti_msp430pack_setup64_11.0.0.exe --prefix "D:\ti\ccs1100/ccs" --eclipseprefix "D:/ti/ccs1100/ccs/eclipse"--mode unattended --installer-log
"D:\ti\ccs1100/ccs/install_logs/20211206151047"--ccs true: child killed:unknown signal
The application will exit now.

However, the C2000 components can be installed properly. The operating system is Windows 11, Professional Insider Preview Dev 22509.1011 This installation file is capable of installing the MSP430 or MSP432 components on previous Windows 11 before reinstalling the system. The install log is as follows:
Could you help check this case? Thanks.
Best Regards,
Cherry