This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6043: To increasing the sampling frequency of Delta_TOF

Part Number: EVM430-FR6043

Hi team,

Customers are now evaluating the gas ultrasonic flow module using the EVM430-FR6043 platform. The Delta_TOF sampling frequency of 150 hz is required in real-world applications and can currently be set to only up to 20 hz with USSSWLIB software debugging (the minimum time from UPS0 to UPS1 can be set to 50 ms extrapolation).

Issue: the customer would like to know why the minimum limit is 50 ms. The initial assumption may be that the soft run time is large, so what is the actual operating time of the hibernate wide and is it possible to optimize?

Could you help check this case? Thanks.

Best Regards,

Cherry

**Attention** This is a public forum