Part Number: MSP430FR2433
Sections 5.4 and 5.5 of the data sheet (SLASE59) specify the AM supply current. Why don't the specifications in 5.4 equal to some multiple of Current Per MHz shown in section 5.5?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR2433
Sections 5.4 and 5.5 of the data sheet (SLASE59) specify the AM supply current. Why don't the specifications in 5.4 equal to some multiple of Current Per MHz shown in section 5.5?
The test conditions for 5.5 are different than 5.4 including the cache hit rate, which is an important factor as you can see comparing the 0% and 100%.
Yes. I saw that.
I find it misleading that section 5.5 uses a hit rate of 75% instead of 100% as used in section 5.4.
The numbers just don't add up to me. Maybe it's because 5.4 uses an external clock signal.
I'll explain a little further here to provide more clarity on to how the numbers were calculated. Keep in mind the test conditions.
There is always some current that is there, this current could be the b in the linear formula y = mx+b, this could be the leakage current of the system. Now to calculate the slope we had Iam at 8 MHz and Iam at 1 MHz (with 75% cache hit rate for both) then we divided by 7 for the difference. Using the number from 5.4 and the equation from 5.5 we can get the supply current per MHz.
| 1 MHz | 8MHz | Unit | |
| Iam Current Cache 0% | 504 | 2772 | uA |
| Iam Current Cache 100% | 203 | 625 | uA |
| Iam Current Cache 75% | 278.25 | 1161.75 | uA |
| 0% Value(0.25) + 100% Value (0.75) | |||
| Calculated Value | |||
| (Iam 8 MHz - Iam 1 MHz) / 7 | 126.2143 | uA/MHz | |
Its important to note that this gives you the slope, but there is also the leakage current and the 75% cache hit rate.
Regards,
Luke
**Attention** This is a public forum