This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6736: Chip accuracy issue

Part Number: MSP430F6736

Hi team,

MSP430F6736IPZ chip with single-phase meter in use, 220V, 10 (80) A. The ultimate voltage impact test is currently being performed, applying 120% Un, 70% Un and Un voltages on the voltage line, measuring the maximum error change at power factor 1.0 and 0.5 L. At 1.2 Un, is 1.0, the error change of 5% points was -1.03%.

The customer would like to know whether this is related to the accuracy of this chip. Could you help check this case? Thanks.

Best Regards,

Cherry

**Attention** This is a public forum