This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F249: DCO setting and wait time

Guru 12915 points
Part Number: MSP430F249


Hi,

I have a question about setting the clock.

1) I would like to know how to set MCLK to 12MHz using DCO.

2) It is assumed that the DCO clock is set immediately after "Stop WDT".
Do I need to wait before setting the DCO?

3)

How is the frequency switching of DCO performed as a circuit?

Thanks,

**Attention** This is a public forum