Other Parts Discussed in Thread: CC1310, MSP430FR2475, MSP430FR2155, MSP430FR5962
1、Can you provide a similar model of CC1310? That is, all function configurations of CC1310 are guaranteed, except RF function is not required) :
1) Interface: UART*1 + IIC*1 + SPI*1;
2) FALSH: 32KB, not considering firmware upgrade;
3) RAM: 16KB;
4) GPIO: no less than 10 channels;
5) Main frequency: 8MHz, using external crystal oscillator;
2. MCU requirements at the aggregation end (1-2 specifications and models are recommended) :
1) Interface: UART*2 + IIC*1 + SPI*2;
2) FALSH: 128KB, BLOCK addressing capacity is 2KB;
3) RAM: 64K;
4) GPIO: no less than 10 channels;
5) Main frequency: 24MHz, using external crystal oscillator;