This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XCAP settings

Other Parts Discussed in Thread: MSP430F5437

Dear forum members,

I need a clarification: We are using the MSP430F5437 with a 32Khz crystal (Crystal load capacitance as it appears in the datasheet = 12pF).

Do I need to add external capacitors or can I just set the XCAP settings to XCAP=3 (CL=12pF)?

 

Thanks in advance,

 

Assaf

**Attention** This is a public forum