Part Number: MSP430F5659
Hi Sir,
Our customer reported that they use MSP430F5659 to connect to the G-SENSOR chip through the P2.7/P2MAP7 pin, and G_EN will instantly cause the MSP430F5659 to restart abnormally. From the log information, we can know that the restart is mainly manifested as 0x02h, 0x04h, 0x20h appear in SYSRSTIV Register.
The specific problem description is that when the system power is turned on, the G-EN is enable and then the MCU will restart. But if we re-powered on immediately, it will be able to start normally. We have tried to remove U23 and just connect R70 for MCU_vcc for power supply, the same problem will occur.
The schematic of MSP430F5659 connected with G-SENSOR is as follows:


The SYSRSTIV Register description.

Can u give us some suggestion for this problem?
Thanks,
Best Regards