Part Number: MSP-EXP430FR2433
Other Parts Discussed in Thread: MSP430WARE
Problem: I want to use UART on UCA0 and SPI on UCA1. Joined examples from driverlib library. Once SPI is initialized, UART starts to work incorrectly.
Code:
#include "driverlib.h"
#include "Board.h"
#include "stdio.h"
#define STR_LEN 100
char str[STR_LEN];
uint8_t RXData = 0;
uint8_t check = 0;
void initClocks(void);
void initGpio(void);
void initSPI(void);
void sendUartMsg(char* str);
void initUart(void);
uint8_t stringLength(char* str);
void main(void)
{
//Stop Watchdog Timer
WDT_A_hold(WDT_A_BASE);
initClocks();
initGpio();
// clocks should be initialized
// appropriately
initUart();
initSPI();
// Enable global interrupts
__enable_interrupt();
while (1)
{
sprintf(str, "abcdef\r\n");
sendUartMsg(str);
sprintf(str, "a\r\n");
sendUartMsg(str);
_delay_cycles(100000);
}
return;
}
void initClocks(void) {
//Set ACLK = REFOCLK with clock divider of 1
CS_initClockSignal(CS_ACLK,CS_REFOCLK_SELECT,CS_CLOCK_DIVIDER_1);
//Set SMCLK = DCO with frequency divider of 1
CS_initClockSignal(CS_SMCLK,CS_DCOCLKDIV_SELECT,CS_CLOCK_DIVIDER_1);
//Set MCLK = DCO with frequency divider of 1
CS_initClockSignal(CS_MCLK,CS_DCOCLKDIV_SELECT,CS_CLOCK_DIVIDER_1);
}
void initGpio(void) {
//Configure UART pins
GPIO_setAsPeripheralModuleFunctionInputPin(
GPIO_PORT_UCA0TXD,
GPIO_PIN_UCA0TXD,
GPIO_FUNCTION_UCA0TXD
);
GPIO_setAsPeripheralModuleFunctionInputPin(
GPIO_PORT_UCA0RXD,
GPIO_PIN_UCA0RXD,
GPIO_FUNCTION_UCA0RXD
);
GPIO_setAsPeripheralModuleFunctionInputPin(
GPIO_PORT_P2,
GPIO_PIN4 + GPIO_PIN5 + GPIO_PIN6,
GPIO_PRIMARY_MODULE_FUNCTION
);
PMM_unlockLPM5();
}
void initUart(void) {
//Configure UART
//SMCLK = 1MHz, Baudrate = 115200
//UCBRx = 8, UCBRFx = 0, UCBRSx = 0xD6, UCOS16 = 0
EUSCI_A_UART_initParam param = {0};
param.selectClockSource = EUSCI_A_UART_CLOCKSOURCE_SMCLK;
param.clockPrescalar = 8;
param.firstModReg = 0;
param.secondModReg = 0xD6;
param.parity = EUSCI_A_UART_NO_PARITY;
param.msborLsbFirst = EUSCI_A_UART_LSB_FIRST;
param.numberofStopBits = EUSCI_A_UART_ONE_STOP_BIT;
param.uartMode = EUSCI_A_UART_MODE;
param.overSampling = EUSCI_A_UART_LOW_FREQUENCY_BAUDRATE_GENERATION;
if (STATUS_FAIL == EUSCI_A_UART_init(EUSCI_A0_BASE, ¶m)) {
return;
}
EUSCI_A_UART_enable(EUSCI_A0_BASE);
EUSCI_A_UART_clearInterrupt(EUSCI_A0_BASE,
EUSCI_A_UART_RECEIVE_INTERRUPT);
// Enable USCI_A0 RX interrupt
EUSCI_A_UART_enableInterrupt(EUSCI_A0_BASE,
EUSCI_A_UART_RECEIVE_INTERRUPT);
}
void sendUartMsg(char* str) {
uint8_t i;
uint8_t length = stringLength(str);
char curChar;
for (i = 0; i < length; ++i) {
curChar = str[i];
//need to print first symbol correctly
_delay_cycles(10000);
// Load data onto buffer
EUSCI_A_UART_transmitData(EUSCI_A0_BASE, curChar);
}
}
uint8_t stringLength(char* str) {
uint8_t i = 0;
while (str[i] != '\0') {
i++;
}
return i;
}
void initSPI(void) {
//Initialize Master
EUSCI_A_SPI_initMasterParam param = {0};
param.selectClockSource = EUSCI_A_SPI_CLOCKSOURCE_SMCLK;
param.clockSourceFrequency = CS_getSMCLK();
param.desiredSpiClock = 500000;
param.msbFirst = EUSCI_A_SPI_MSB_FIRST;
param.clockPhase = EUSCI_A_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT;
param.clockPolarity = EUSCI_A_SPI_CLOCKPOLARITY_INACTIVITY_LOW;
param.spiMode = EUSCI_A_SPI_3PIN;
EUSCI_A_SPI_initMaster(EUSCI_A1_BASE, ¶m);
//Enable SPI module
EUSCI_A_SPI_enable(EUSCI_A1_BASE);
//Clear receive interrupt flag
EUSCI_A_SPI_clearInterrupt(EUSCI_A1_BASE,
EUSCI_A_SPI_RECEIVE_INTERRUPT
);
// Enable USCI_A1 RX interrupt
EUSCI_A_SPI_enableInterrupt(EUSCI_A1_BASE,
EUSCI_A_SPI_RECEIVE_INTERRUPT);
}
CCS Version: 11.0.0.00012
OS: Ubuntu
Thnaks in advance ;)