Other Parts Discussed in Thread: MSP430FR2355
Hello everybody
I am using with MSP430FR2355, I need to measure frequency from the frequency divider in 4Mhz and capture it.
I tested 2 sample code ( MSP4302235X_tb0_capture.c and MSP4302235X_tb0_22.c) , now I have question's:
1- I am using MSP430Fr2355 Launchpad and I don't have access to Pin 2.7 for as a input, what should I do now?
2- I should use TB0CLK for timer and TB0TRG for trigger? could you please explain it what should I do.
3- Do I need to connect pins together for timer and trigger?? Because in this link connected 2 pins for timer and trigger together.
Best